Inside the New LED Retrofit Bulbs
Colaboración de Electronic Products
2012-01-31
The first LED replacements for 60 W incandescent bulbs are now appearing on shelves in local stores across the United States. Although current U.S. law will phase out only 100 W incandescent bulbs in 2012, one can easily find replacements for incandescent bulbs of other wattages – 15, 25, 40, 60, and 75. The initial cost of the LED bulbs is relatively high, but they more than pay for themselves over time with their longevity and energy savings.
The LED bulb that has received the most attention so far is the AmbientLED Model 12E26A60, a 12.5 W, 800-lm replacement for 60 W incandescent bulbs made by Philips Lighting (Figure 1). It is similar in configuration to the bulb that won the U.S. Department of Energy’s first Bright Tomorrow Lighting competition, or L Prize. It was also declared a standout among the CFL and LED bulbs in lamp and ceiling fixture tests conducted by Consumer Reports magazine.

At first glance, these yellow-orange-colored bulbs do not look like they would produce the 2,700 K warm-white light we’ve come to expect from a typical household incandescent bulb. That’s because the LED bulb’s outer plastic surface has a remote-phosphor coating on its inside, which is actually key to its performance. The phosphor efficiently converts the light of high-efficacy blue LEDs into warm-white light while simultaneously making the lighting even across the surface.
Intematix Corp.’s ChromaLit remote phosphor technology (Figure 2) is commercially available in various shapes and sizes. Thus designers can easily make use of the technology for whatever lighting designs they may be considering.

The bulb actually uses three sets of six blue LEDs. In each of the three portions of the lamp, the LEDs are set on a board that is held in place against the heat sink by a plastic frame that is screwed to the heat sink. A piece of thermally conductive padding sits between the board and the heat sink.
Cree recently introduced the XLamp XT-E Royal Blue LED (Figure 3), a high performing source of blue light for remote phosphor applications that the company says sets new standards of efficiency and light extraction in royal blue LEDs. Compared to the standard XLamp XP-E Royal Blue, the XT-E Royal Blue is up to 20 percent more efficient, and is available with minimum radiant flux of 475 or 500 mW when operated with a 350-mA driving current and a high, but realistic, junction temperature of 85°C.

Lighting boards
The LED lighting boards all have connectors which provide a more reliable design than simple soldered wire. The leads from the boards go through the center of the heat sink to connectors on a small board that is connected to the lamp’s driver electronics system (Figure 4). The AmbientLED is designed to work with standard dimmer circuits, and so requires more than a simple AC/DC converter.
On one side of the driver board are the capacitors, inductor coils, and heavy-duty resistors. On the opposite side of the board are the driver chip, chip resistors and capacitors that take on the digital functions needed to control the LEDs. The triac-dimmer-adjusted 60-Hz AC signal coming into the lamp is converted by the driver into a Pulse Width Modulation (PWM) signal that turns the LEDs ON and OFF for variable amounts of time. The switching frequency is high enough that the human eye does not perceive any flicker, yet the eye sees the decrease in light output as a continuous even dimming.

The dimmer used here is a CY8CLED EZ-Color high-brightness (HB) LED controller from Cypress Semiconductor. The EZ-Color family of devices was designed to offer powerful, highly flexible control solutions for high brightness LED applications requiring intelligent dimming control. The devices combine Cypress's Programmable System-on-Chip (PSoC) with its precise illumination signal modulation (PrISM) modulation technology to create a fully customizable and integrated lighting solution platform.
The EZ-Color family supports a range of independent LED channels -- from 4 channels at 32 bits of resolution each, up to 16 channels at 8 bits of resolution each -- to let designers choose the most suitable LED array size and color quality for their application. PSoC Designer software, with lighting specific drivers, can significantly cut development time and simplify implementation of fixed color points through temperature, optical, and LED binning compensation. EZ-Color's broad analog and digital customization capability enable simple integration of features in addition to intelligent lighting.
More to come
While the AmbientLED has enjoyed an early success, it is unlikely to be the final word in incandescent replacement bulbs. Indeed, both Cree and General Electric have unveiled LED bulb designs which they hope will also receive the approval of the DoE. With the wide availability of components for LED bulbs, practically any designer can try his or her hand at inventing the next light bulb.
Descargo de responsabilidad: Las opiniones, creencias y puntos de vista expresados por los autores o participantes del foro de este sitio web no reflejan necesariamente las opiniones, las creencias y los puntos de vista de DigiKey o de las políticas oficiales de DigiKey.