Capacitor Characteristics Impact Energy Harvesting Efficiency

Por Stephen Evanczuk

Colaboración de Electronic Products


For energy harvesting, capacitor selection requires careful consideration of characteristics beyond simple capacitance value. Among these characteristics, leakage current remains a primary concern. Today, however, designers can find options ranging from low-leakage electrolytic capacitors to high-performance supercapacitors from manufacturers including AVX, Kemet, Maxwell Technologies, Murata, NessCap, Seiko Instruments, Taiyo Yuden, and United Chemi-Con, among others.

Capacitors often show up as an afterthought in many design situations, added to circuits to clean up signals and power sources. In signal acquisition, capacitors play a more central role in filtering out-of-band sources and in sample-and-hold stages for analog/digital converters. In energy-harvesting applications, however, capacitors provide a critical component for accumulating charge from low-energy ambient sources and discharging stored charge quickly and efficiently into a load. In these applications, capacitor characteristics and component selection rise as vital factors in design.

In their traditional roles in circuit design, capacitors are considered as constant capacitance components for filtering, decoupling, and any of the other familiar uses for these devices. For those purposes, differences between the characteristics of an ideal capacitor and those of a real capacitor typically do not greatly impact their ability to fill their role adequately. For energy-harvesting applications, however, the departure from an ideal capacitor significantly impacts the efficiency of the design as a whole.

Among common effects (Figure 1), equivalent-series resistance (ESR) and leakage current dominate an array of non-ideal characteristics that can degrade efficiency. High ESR causes a capacitor to dissipate power, particularly when subject to high AC currents. As such, the use of low-ESR capacitors results in overall higher efficiency in an energy-harvesting subsystem. Leakage current exerts a more profound effect in designs using very-low-energy ambient sources — and rises as a significant limitation in the ability to apply more familiar types of capacitors in energy-harvesting designs.

Image of Analog Devices ESR and parallel resistance

Figure 1: In energy-harvesting applications, equivalent-series resistance (ESR) and parallel resistance (RL) result in power loss that erodes overall efficiency. (Courtesy of Analog Devices)

For any capacitor, the amount of leakage current depends on a variety of factors and changes with time, voltage, and temperature (Figure 2). From the moment it is fully charged, a capacitor exhibits a relatively large current flow initially until it eventually reaches a lower constant value. As a result of the time required to reach this constant level, industry practice typically relies on measurements for leakage current taken after only a few minutes. Because of the difficulties in quantifying non-ideal behavior of a capacitor, some manufacturers will combine leakage current, ESR, and ESL into a single value called the dissipation factor, which is defined as ratio of energy dissipated per cycle to energy stored per cycle — in effect, a measure of the inefficiency of a capacitor.

Image of Vishay leakage current in capacitors

Figure 2: Leakage current in capacitors depends on a variety of factors, including time (A), voltage (B), and temperature (C). (Courtesy of Vishay)

Leakage current also increases with the operating voltage (UB in Figure 2B); rising significantly as applied voltage exceeds the rated voltage (UR in Figure 2B) and passes the surge voltage US and eventually the preforming voltage (UF in Figure 2B) of the capacitor anode. At levels above the surge voltage, physical and chemical reactions can occur in the capacitor. As a result, capacitors are typically not operated at levels above the rated voltage. Finally, leakage current can increase with rising ambient temperature due to the effects of temperature on physical and chemical reactions in capacitors.

Leakage current is characteristic to all capacitor types, but some types have traditionally exhibited greater leakage current than others. For example, electrolytic capacitors remain the workhorse of design but their leakage characteristics have been a concern for use in designs with limited power budgets. Offering high-capacitance values and an ability to handle high voltages and currents, electrolytic capacitors fill a role ranging from use as a basic decoupling or filtering component in traditional design work to use in power conditioning stages in solar inverters.

In the past, electrolytic capacitors exhibited significant leakage current that largely precluded their use in energy harvesting from weak energy sources. Today, however, advances in materials science and manufacturing have enabled manufacturers to deliver tantalum-MnO2 capacitor lines that exhibit significantly lower leakage current. For example, capacitors in the AVX TRJ line or the Kemet T491 line feature leakage current in the low tens of nanoamps.

While more advanced tantalum electrolytic capacitors can meet efficiency requirements in energy-harvesting designs, other capacitor technologies such as film capacitors and ceramic capacitors offer a combination of small package size and performance efficiency (Figure 3). Along with lower ESR, these devices typically feature longer lifetime ratings and lower leakage current than comparable electrolytics. For example, the AVX 1206YD226MAT2A ceramic capacitor exhibits leakage currents below 10 nA (at 3.5 V) and ESR around 800 mOhm (100 Hz). Ceramic capacitors also feature very tight tolerances; for example, the Murata GRM ceramic capacitor series includes parts such as the GRM0335C1ER10WA01D that feature a tolerance of ±0.05 pF.

Image of Murata impedance Z and equivalent series resistance of capacitors

Figure 3: The impedance Z and equivalent series resistance (ESR) of capacitors can vary dramatically across frequency and capacitor type. (Courtesy of Murata)

For many energy-harvesting applications, electric-double-layer capacitors (EDLC), or supercapacitors, have emerged as the preferred solution, providing a combination of high capacitance, efficiency, and small package size that conventional capacitor technologies are rarely able to match. Supercapacitor families such as the Maxwell Technologies K2, United Chemi-Con DLCAP, and NessCap UltraCap offer ESR below 1 mOhm with capacitance values starting at 650 F in 60 mm x 72 mm and larger packages. At the same time, designers looking for a smaller design footprint can find supercapacitors that offer significant capacitance values in very small packages. For example, the Seiko Instruments CPH3225A and Taiyo Yuden PAS series feature 11 mF and 14 mF components in 3.2 mm x 2.5 mm packages.

Although supercapacitors offer superior energy density, their characteristic curves can be much more complex. Supercapacitors combine several capacitors, which can each contribute to a relatively significant total leakage current for a particular device (Figure 4). As a result, designers can find they need to accept a degree of energy loss due to leakage current to gain the exceptionally-high-density energy-storage capacity available with these components.

Image of Murata supercapacitors built up from multiple capacitors

Figure 4: Supercapacitors are built up from multiple capacitors (A) that each contribute to overall leakage current (B). (Courtesy of Murata)

In summary, unlike conventional applications, designs that harvest energy from low-energy ambient sources require components that themselves consume little power during operation. Although designers might have disqualified electrolytic capacitors in the past because of their relatively-high-leakage current, manufacturers today offer electrolytic capacitors with characteristics well matched to many energy-harvesting applications. While alternate technologies, such as film capacitors and ceramic capacitors offer improved characteristics, compact size and high capacitance, supercapacitors deliver high-energy density at the cost of higher leakage and ESR.

For more information about the parts discussed in this article, use the links provided to access product information pages on the DigiKey website.

 

Descargo de responsabilidad: Las opiniones, creencias y puntos de vista expresados por los autores o participantes del foro de este sitio web no reflejan necesariamente las opiniones, las creencias y los puntos de vista de DigiKey o de las políticas oficiales de DigiKey.

Acerca de este autor

Image of Stephen Evanczuk

Stephen Evanczuk

Stephen Evanczuk tiene más de 20 años de experiencia escribiendo para y sobre la industria de electrónica en un amplio rango de temas, entre ellos hardware, software, sistemas y aplicaciones, que incluyen IoT. Se doctoróen neurociencias (redes neuronales) y trabajó en la industria aeroespacial en sistemas seguros con distribución masiva y métodos de aceleración de algoritmos. Actualmente, cuando no escribe artículos sobre tecnología e ingeniería, trabaja en aplicaciones de aprendizaje profundo sobre sistemas de reconocimiento y recomendaciones.

Acerca de este editor

Electronic Products

La revista Electronic Products y ElectronicProducts.com ofrece ingenieros y gerentes de ingeniería responsables de diseñar equipos y sistemas electrónicos.