Mediante el uso de la iluminación LED, la NASA ha descubierto cómo hacer que la comida espacial sea más sabrosa.
Así es como la Universidad de Minnesota y DigiKey colaboraron para lanzar rápidamente al mercado un respirador de consumo masivo que puede utilizarse en pacientes con COVID-19.
Los módulos de potencia PFH500 de TDK-Lambda cumplen con los criterios de diseño industrial para entornos difíciles.
Comprender y aplicar IO-Link para implementar sensores y actuadores inteligentes y comunicarse con ellos de manera eficiente y rentable en una aplicación de IIoT.
Agregar sensores a los drones requiere de un especial equilibrio entre el consumo de energía, la funcionalidad y el costo, pero aquí ofrecemos algunas opciones compatibles.
El MPPT, la monitorización remota del sensor y un transistor GaN en un PoL de suministro de energía PoL se encuentran entre las opciones que los diseñadores pueden usar para hacer una copia de seguridad de un sistema de energía basado en la IA, por si acaso.
Almost three decades ago, the "brick" DC/DC converter power module was developed, which eventually led to the distributed power architecture (DPA) becoming the de facto standard for point of load (POL) designs.
Home energy systems based on renewable sources, such as solar and wind power, are becoming more popular among consumers and will gain increasing support from governmental bodies.
Flow sensors are used to measure flow velocity, volumetric flow rate, or mass flow of a liquid or gas. Mass flow for gases is specified in units of standard liters per minute (slm) or standard cubic centimeters per minute (sccm).
What once was a straightforward act of transforming an AC waveform into a DC source to power downstream devices is now greatly affected and driven by the power grid to maximize its available power.
Powerline filters protect expensive circuitry from potentially damaging power surges, as well as protecting the AC line from excessive noise conducted back into it from a noisy power converter.
Modular, high-density POL (point-of-load) power DC/DC converters have some excellent advantages over other power management architectures.
DC/DC converters are a great high-frequency noise source. Designers must take careful steps to minimize and contain this noise near and around the converter to keep it from affecting other system components or the AC mains.
Battery size constraints in energy harvesting systems necessitate creativity and innovation in order to maximize efficiency of the power source.
Ambient light sensor (ALS) products are quickly becoming one of the most effective solutions for power management and display quality enhancement in electronic products and systems.
As newer applications and systems tend to have multiple voltages to power DSPs, µCs, FPGAs, and ASICs, modern power supply designs must be able to control how and when these voltages ramp to their final values after the power switch is activated.
Relative humidity (RH) is defined as the ratio of the partial pressure of water vapor (in a gaseous mixture of air and water vapor) to the saturated vapor pressure of water at a given temperature.
Designers using modular power converters for their systems know how critical a thermal derating curve is to the success of their design.
Need a temperature sensor for your next application? You'll first need to sort through the three-letter acronyms before arriving at any BOMs.
A gas detection sensor’s function is to measure the concentration of gases. These devices have different methods to convert the gas detection element’s output to voltage.