Maker.io main logo

NeoAnim Using Bitmaps to Animate NeoPixels on Circuit Playground

129

2016-12-13 | By Adafruit Industries

License: See Original Project

Courtesy of Adafruit

Guide by John Park

From Pixels to NeoPixels

Lighting up NeoPixels on the Circuit Playground is fun and easy. But creating animation patterns with specific color, timing, and position can be difficult. Not any more! Using this technique and a small Python script, you can use a tiny bitmap image as a powerful control for making complex NeoPixel animations on your Circuit Playground.

Developed by our own Phil Burgess, this method has a lot in common with traditional hand-drawn animation timing charts and exposure sheets (also called dope sheets) in that a set of rows and columns are used to indicate an object's attributes over time.

Neo Anim: Using Bitmaps to Animate Neo Pixles

Neo Anim: Using Bitmaps to Animate Neo Pixles

Neo Anim: Using Bitmaps to Animate Neo Pixles

In this example of animating a ball bounce in Maya, note the dope sheet interface where the translation, rotation, and scale values of the ball are the attributes being indicated on the vertical chart axis, and the time in frames are the horizontal axis. This is very similar to our bitmap-to-NeoPixel animation system.

Neo Anim: Using Bitmaps to Animate Neo Pixles

In this case, rows indicate each of the ten NeoPixels of the Circuit Playground, and columns represent frames of animation in time. The color of a particular cell in the grid represents what color to display that NeoPixel at that frame in time.

Here's an example: This is a one second loop of animation divided into 24 frames per second (24 FPS) which is the standard for traditional film and animation. In the image above, the ten NeoPixels (numbered 0-9) will each be lit green for one frame of time until NeoPixel 9 is lit, which then stays lit for the rest of the animation loop.

Neo Anim: Using Bitmaps to Animate Neo Pixles

Here's what happens when the pixels are changed to red.

Neo Anim: Using Bitmaps to Animate Neo Pixles

Neo Anim: Using Bitmaps to Animate Neo Pixles

Now, let's combine two sets of pixel motion together.

Neo Anim: Using Bitmaps to Animate Neo Pixles

Neo Anim: Using Bitmaps to Animate Neo Pixles

We can also use things like gradients in Photoshop or other image editing software to create gentle fades or color transformations. Here's a one second fade up to blue and back.

Neo Anim: Using Bitmaps to Animate Neo Pixles

Neo Anim: Using Bitmaps to Animate Neo Pixles

Take a look at a rotated gradient bar. Notice how it doesn't loop smoothly, or hook-up properly in animation terms.

Neo Anim: Using Bitmaps to Animate Neo Pixles

Neo Anim: Using Bitmaps to Animate Neo Pixles

Here's one way to fix that, by blending the tail back to the head in the bitmap.

Neo Anim: Using Bitmaps to Animate Neo Pixles

Neo Anim: Using Bitmaps to Animate Neo Pixles

This fixes the hookup, but it's very fast. We can make a wider input bitmap to give us more frames of animation. This one is now 48 pixels wide, which translates to two seconds at 24FPS.

Neo Anim: Using Bitmaps to Animate Neo Pixles

Neo Anim: Using Bitmaps to Animate Neo Pixles

For a continuous sweep, we'll need to be more careful with the transitions and only "travel" the graphic in one direction.

Neo Anim: Using Bitmaps to Animate Neo Pixles

Neo Anim: Using Bitmaps to Animate Neo Pixles

Noise can also be effective for creating sparkling, blinking animation. Here's a short 12 frame cycle.

Neo Anim: Using Bitmaps to Animate Neo Pixles

Neo Anim: Using Bitmaps to Animate Neo Pixles

Wider input bitmaps give you more time to play with animation patterns.

Neo Anim: Using Bitmaps to Animate Neo Pixles

Neo Anim: Using Bitmaps to Animate Neo Pixles

We can also use acceleration curves, such as this example. Each "drop" is shorter in number of frames than the last as the lights accumulate on the opposite side of the starting point.

Neo Anim: Using Bitmaps to Animate Neo Pixles

Neo Anim: Using Bitmaps to Animate Neo Pixles

Next we'll take a look at how to set up the Circuit Playground and convert bitmaps to animation header files.

Coding the Circuit Playground

Before you get started, make sure you've been through the basic tutorials on using the Circuit Playground. You'll need to have installed the Arduino IDE, added the Circuit Playground board to Arduino, and added the Circuit Playground library. This excellent guide, Introducing Circuit Playground and Circuit Playground lesson #0 will show you how to do all of that and get you going.

Neo Anim: Using Bitmaps to Animate Neo Pixles

Plug your Circuit Playground into your computer now, and launch the Arduino IDE. Double check that you've selected the board and port as in the Lesson #0 tutorial and are ready to upload code.

Download the NeoAnim.zip Arduino sketch, then unzip it, and place the NeoAnim directory in your Arduino sketch directory.

NeoAnim.zip

The directory contains the NeoAnim.ino Arduino sketch, a 24x10 pixel neoAnim.png bitmap file, and the neoAnim.h header file that was created with the convert.py Python script we'll look at in a few steps.

Copy Code
//NeoAnim for Circuit Playground
// adapted by John Park from Circuit Playground Make Believe by Phil Burgess
// for Adafruit Industries
// MIT License

#include <Adafruit_CircuitPlayground.h>
#include "neoAnim.h" //this is the name of the animation derrived from the neoAnim.png bitmap file


void setup() {
// Initialize Circuit Playground board, NeoPixels
CircuitPlayground.begin();
CircuitPlayground.strip.setBrightness(20);

// Start looping animation
playAnim( neoAnimPixelData, neoAnimFPS , sizeof(neoAnimPixelData), true);
}

// Global values used by the animation and sound functions
uint16_t *pixelBaseAddr, // Address of active animation table
pixelLen, // Number of pixels in active table
pixelIdx, // Index of first pixel of current frame
audioLen; // Number of audio samples in active table
volatile uint16_t audioIdx; // Index of current audio sample
uint8_t pixelFPS, // Frames/second for active animation
*audioBaseAddr; // Address of active sound table
boolean pixelLoop, // If true, animation repeats
audioLoop; // If true, audio repeats

// Begin playing a NeoPixel animation from a PROGMEM table
void playAnim(const uint16_t *addr, uint8_t fps, uint16_t bytes, boolean repeat) {
pixelBaseAddr = addr;
if(addr) {
pixelFPS = fps;
pixelLen = bytes / 2;
pixelLoop = repeat; //if set to 'repeat' it'll loop, set to 0 to play once only
pixelIdx = 0;
} else {
CircuitPlayground.strip.clear();
}
}

uint32_t prev = 0; // Time of last NeoPixel refresh

void loop() {
uint32_t t; // Current time in milliseconds

// Until the next animation frame interval has elapsed...
while(((t = millis()) - prev) < (1000 / pixelFPS));
// Show LEDs rendered on prior pass. It's done this way so animation timing
// is a bit more consistent (frame rendering time may vary slightly).
CircuitPlayground.strip.show();


prev = t; // Save refresh time for next frame sync

if(pixelBaseAddr) {
for(uint8_t i=0; i<10; i ) { // For each NeoPixel...
// Read pixel color from PROGMEM table
uint16_t rgb = pgm_read_word(&pixelBaseAddr[pixelIdx ]);
// Expand 16-bit color to 24 bits using gamma tables
// RRRRRGGGGGGBBBBB -> RRRRRRRR GGGGGGGG BBBBBBBB
CircuitPlayground.strip.setPixelColor(i,
pgm_read_byte(&gamma5[ rgb >> 11 ]),
pgm_read_byte(&gamma6[(rgb >> 5) & 0x3F]),
pgm_read_byte(&gamma5[ rgb & 0x1F]));
}


if(pixelIdx >= pixelLen) { // End of animation table reached
if(pixelLoop) { // Repeat animation
pixelIdx = 0; // Reset index to start of table
} else { // else switch off LEDs
playAnim(NULL, neoAnimFPS, 0, false);
}
}

}
}

Next, you'll download the code that'll allow you to convert bitmaps to animation header files, and play these NeoPixel animations on your Circuit Playground.

Circuit Playground Make Believe

Download the linked code from the button above, and then unzip the directory. Within the unzipped directory you'll find two directories: CircuitPlaygroundMakeBelieve, which you can move to your Arduino sketch directory (we won't use it for this guide, but it is useful if you want to build reactive props as shown in this guide), and the Extras directory, which you can place inside your NeoAnim directory you previously downloaded.

You can test the NeoAnim Arduino sketch by opening it in Arduino, and uploading it to your Circuit Playground. It should play a one second loop of a green pixel moving from upper left to upper right counterclockwise.

Now, you can adjust the animation. Open the neoAnim.png file in an image editor, such as Preview on OSX or MS Paint on Windows, or GIMP on Linux, and make some changes, such as the color of the non-black pixels. Save the file (it's OK to overwrite, you can redownload the original here).led_pixels_neoAnim.png

In order to convert the new version of neoAnim.png to the neoAnim.h file, you'll need to follow these steps:

     1. Install Python 3.5 https://www.python.org/downloads/
     2. Add the Pillow or PIL imaging library to Python http://pillow.readthedocs.io/en/3.0.x/installation.html
     3. Open a command shell and navigate to the NeoAnim directory inside your Arduino sketches directory
     4. type the command to convert the bitmap: python convert.py neoAnim.png > neoAnim.h

This will generate the animation header file that looks something like this (yours will vary depending on the colors and placements of pixels):

Copy Code
#define neoAnimFPS 30

const uint16_t PROGMEM neoAnimPixelData[] = {
0X07E0, 0X0000, 0X0000, 0X0000, 0X0000, 0X0000, 0X0000, 0X0000, 0X0000,
0X0000, 0X0000, 0X07E0, 0X0000, 0X0000, 0X0000, 0X0000, 0X0000, 0X0000,
0X0000, 0X0000, 0X0000, 0X0000, 0X07E0, 0X0000, 0X0000, 0X0000, 0X0000,
0X0000, 0X0000, 0X0000, 0X0000, 0X0000, 0X0000, 0X07E0, 0X0000, 0X0000,
0X0000, 0X0000, 0X0000, 0X0000, 0X0000, 0X0000, 0X0000, 0X0000, 0X07E0,
0X0000, 0X0000, 0X0000, 0X0000, 0X0000, 0X0000, 0X0000, 0X0000, 0X0000,
0X0000, 0X07E0, 0X0000, 0X0000, 0X0000, 0X0000, 0X0000, 0X0000, 0X0000,
0X0000, 0X0000, 0X0000, 0X07E0, 0X0000, 0X0000, 0X0000, 0X0000, 0X0000,
0X0000, 0X0000, 0X0000, 0X0000, 0X0000, 0X07E0, 0X0000, 0X0000, 0X0000,
0X0000, 0X0000, 0X0000, 0X0000, 0X0000, 0X0000, 0X0000, 0X07E0, 0X0000,
0X0000, 0X0000, 0X0000, 0X0000, 0X0000, 0X0000, 0X0000, 0X0000, 0X0000,
0X07E0, 0X0000, 0X0000, 0X0000, 0X0000, 0X0000, 0X0000, 0X0000, 0X0000,
0X0000, 0X07E0, 0X0000, 0X0000, 0X0000, 0X0000, 0X0000, 0X0000, 0X0000,
0X0000, 0X0000, 0X07E0, 0X0000, 0X0000, 0X0000, 0X0000, 0X0000, 0X0000,
0X0000, 0X0000, 0X0000, 0X07E0, 0X0000, 0X0000, 0X0000, 0X0000, 0X0000,
0X0000, 0X0000, 0X0000, 0X0000, 0X07E0, 0X0000, 0X0000, 0X0000, 0X0000,
0X0000, 0X0000, 0X0000, 0X0000, 0X0000, 0X07E0, 0X0000, 0X0000, 0X0000,
0X0000, 0X0000, 0X0000, 0X0000, 0X0000, 0X0000, 0X07E0, 0X0000, 0X0000,
0X0000, 0X0000, 0X0000, 0X0000, 0X0000, 0X0000, 0X0000, 0X07E0, 0X0000,
0X0000, 0X0000, 0X0000, 0X0000, 0X0000, 0X0000, 0X0000, 0X0000, 0X07E0,
0X0000, 0X0000, 0X0000, 0X0000, 0X0000, 0X0000, 0X0000, 0X0000, 0X0000,
0X07E0, 0X0000, 0X0000, 0X0000, 0X0000, 0X0000, 0X0000, 0X0000, 0X0000,
0X0000, 0X07E0, 0X0000, 0X0000, 0X0000, 0X0000, 0X0000, 0X0000, 0X0000,
0X0000, 0X0000, 0X07E0, 0X0000, 0X0000, 0X0000, 0X0000, 0X0000, 0X0000,
0X0000, 0X0000, 0X0000, 0X07E0, 0X0000, 0X0000, 0X0000, 0X0000, 0X0000,
0X0000, 0X0000, 0X0000, 0X0000, 0X07E0, 0X0000, 0X0000, 0X0000, 0X0000,
0X0000, 0X0000, 0X0000, 0X0000, 0X0000, 0X07E0 };

const uint8_t PROGMEM gamma5[] = {
0X00, 0X00, 0X00, 0X00, 0X01, 0X02, 0X03, 0X05, 0X07, 0X09, 0X0C, 0X10,
0X14, 0X18, 0X1E, 0X24, 0X2B, 0X32, 0X3B, 0X44, 0X4E, 0X59, 0X65, 0X72,
0X80, 0X8F, 0X9F, 0XB0, 0XC2, 0XD5, 0XE9, 0XFF };

const uint8_t PROGMEM gamma6[] = {
0X00, 0X00, 0X00, 0X00, 0X00, 0X00, 0X00, 0X01, 0X01, 0X01, 0X02, 0X02,
0X03, 0X04, 0X04, 0X05, 0X06, 0X07, 0X09, 0X0A, 0X0C, 0X0D, 0X0F, 0X11,
0X13, 0X15, 0X17, 0X1A, 0X1D, 0X1F, 0X22, 0X26, 0X29, 0X2C, 0X30, 0X34,
0X38, 0X3D, 0X41, 0X46, 0X4B, 0X50, 0X55, 0X5B, 0X61, 0X67, 0X6D, 0X74,
0X7A, 0X81, 0X89, 0X90, 0X98, 0XA0, 0XA8, 0XB1, 0XBA, 0XC3, 0XCC, 0XD6,
0XE0, 0XEA, 0XF4, 0XFF };

This file is referenced when Arduino re-compiles your NeoAnim.ino sketch, so to test it out, simply re-upload the code to your Circuit Playground. You've just animated your own NeoPixel animation using an exposure sheet style bitmap!

In the Arduino IDE you can click on the neoAnim.h tab and change the framerate to 24 FPS if you like, or play around with different framerates to slow down or speed up the the loop.

From here, the rest is in your hands! Try different patterns, gradations, color noise, and so on to see what you can create.

Mfr Part # 3000
CIRC PLAYGROUND CLASS ATMEGA32U4
Adafruit Industries LLC
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.