Maker.io main logo

Graphical Programming IDE Software for Arduino, ESP32, STM32, Raspberry

582

2025-07-17 | By Ron Cutts

License: GNU Lesser General Public License Air Quality Ambient Humidity Temperature Arduino

Step 1: INSTALLATION

Visuino currently has two versions: Standard and Pro. We recommend downloading and installing the Pro version, as it offers more features. Even if you don’t buy a permanent license, you can use it temporarily with a trial license.

Below is a step-by-step guide to installing Visuino and activating the trial license:

Note: At the time of writing, the latest version of Visuino was 8.0.0.146. However, it is recommended that you always download the latest version available, as there will be no compatibility problems.

Installation steps:

  1. Go to the Visuino download page: https://www.visuino.com/downloads/

  2. Download the latest version of Visuino.

  3. Run the installer and follow the instructions. (No additional settings are required.)

See the step-by-step images:

Embedded Image

After downloading, open the compressed file and start the installer, then just click Next, Next, Install.

Embedded Image

Step 2: FIRST PROJECT

After completing the installation, start Visuino.

The first time you run the program, it may take a while to load. This is because Visuino needs to compile some internal files and create a cache of the components.

But before starting the project, let’s get to know the interface and a few other details:

  1. Object Inspector: Displays all the settings for the selected component. This is where you adjust specific properties for each item in your project.

  2. Build Panel: Shows the log of the build process, useful for tracking errors or messages during the build.

  3. Root Component: Represents the board used in the project. By default, Visuino starts with the Arduino UNO selected.

  4. Mini Visualization Panel: Visually displays how the components are connected, providing an overview of the project.

  5. Build button: Generates the build of the current project, converting it into code to be sent to the board.

  6. Upload button: Sends the compiled project directly to the board connected via USB.

  7. Component Palette: Contains all the available components. The icons represent categories, and by clicking on each one, you can see the corresponding components.

  8. Serial Monitor: Works in the same way as the Arduino IDE, allowing you to interact.

  9. Serial Monitor Input: Here, you can send texts.

  10. Platform panel: Here you can install different platforms or update existing ones, but Visuino already does this automatically when necessary.

  11. Libraries Panel: Just like the platform panel, here you can install extra libraries. Visuino does not automatically update libraries.

Embedded Image

Embedded Image

Embedded Image

Embedded Image

I can’t tell you all about the interface, but you’ll get to know it better as we go along.

Let’s now find out a bit about the Root component, i.e., the component that represents the board.

  1. Standard Serial Input of the board: In the case of the Arduino UNO, there is only one.

  2. Input for modules that support the I2C protocol;

  3. Pins: (Input)

  4. Pins: (Outputs)

  5. Pins: (Identification of the Pin on the Board, in addition to the number and type, there is other relevant information such as standard identification for connection, I2C, SPI, Tx)

Embedded Image

Step 3: STARTING THE PROJECT

Now that we know the basics of the interface, it’s time to get down to work and actually start our project!

Let’s create a weather station

Our goal will be to build a simple station that measures air temperature and humidity.

Components needed:

For this project, you will need the following items:

  1. DHT11 humidity and temperature sensor: https://www.digikey.com/en/products/detail/universal-solder-electronics-ltd/26085/16822119

  2. Arduino UNO or compatible: https://www.digikey.com/en/products/detail/arduino/a000066/2784006

With the components in hand, make the connection as shown in the image below:

Embedded Image

  1. Red wire: Connection to the board’s 5V input and Pin 1 of the sensor

  2. Black wire: Connection to the board’s GND input and Pin 4 of the sensor

  3. Yellow wire: Connection to the board’s Analog 1 (Digital 15) input and Pin 2 of the sensor

With the connections made, let’s go back to Visuino and create our project.

Go to the components palette and look for the DHT11 component and drag it into the project.

Click on the sensor output pin and connect it to the Digital [15](AnalogIn[1]) pin as shown in the image below:

Embedded Image

Go back to the components palette and look for Packet, and add the Packet component to the project. See the image below:

Embedded Image

Connect the Out of the Packet component to the In of the board’s Serial[0].

Embedded Image

Select the Packet component and in the Object Inspector, check the Only Modified option and add two elements of type Analog.

Embedded Image

  1. Leave the Only Modified property as True.

  2. Click on the … button to open the elements window; Select the Analog element; Click on the Add button; With the two Analog elements added, let’s configure the first one. button to open the elements window;

  3. Select the Analog element.

  4. Click on the Add button.

With the two Analog elements added, let’s configure the first one, leave it as shown in the image below:

Embedded Image

I left it between 0 and 50, because according to the sensor’s datasheet, it measures between 0~50 ºC.

On the second one, leave it as shown in the image below:

Embedded Image

Close the Elements window, and make the connections between the DHT11 component and the Packet as in the image:

Step 4: TESTING

Now let’s compile the project and upload it to the board, see the image below. If the Serial panel is not expanded, click on the button indicated by the blue arrow to expand it.

Embedded Image

  1. Click on the Serial tab.

  2. Check the Connect on Upload box (it will connect the Serial Monitor when the upload is finished).

  3. Click on the button to upload.

You can see the result in two ways, through Instruments or Scope:

Embedded Image

Step 5: FINAL

So that’s it!

If you’re into Arduino, IoT, and embedded systems, you’ve just learned about a practical and visual way to develop your applications for these platforms.

Visuino makes the process much easier, especially for those who are just starting out or want to speed up prototyping. Now it’s up to you: explore, experiment, and create your own projects!

This article was originally written in Portuguese by Visuino user Swellington Soares.

Read it here: https://www.dio.me/articles/visuino-programe-arduino-sem-escrever-uma-linha-de-codigo-e0e3ba919072

Número de parte del fabricante A000066
ARDUINO UNO R3 ATMEGA328P BOARD
Arduino
$27.60
Ver más Details
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.