UTC-500 Series Startup Manual Datasheet by Advantech Corp

View All Related Products | Download PDF Datasheet
AD\-\NTECH From Vwew Rear View I IE 37 fig
UTC-500 Series Startup Manual 1
Front View Rear View
*Please use only VESA compatible mounting – Detailed
floor stand & wall mount datasheet available to download at
Advantech website.
UTC-500 Series
Startup Manual
UTC-515:
A. Power Switch
B. Antenna Port
C. Line-out
D. Mic-in
E. COM3 (UTC-515A/B only)
F. COM2
G. COM1
H. USB 2.0 x 4 (USB 3.0 x 2 for UTC-515C/E)
I. HDMI Port
J. VGA Port
K. LAN Ports x 2
L. CFast Slot (UTC-515A/B only)
M. DC input
UTC-520:
A. Antenna Port
B. Line-out
C. Mic-in
D. COM3 (UTC-520A/B only)
E. COM2
F. COM1
G. USB 2.0 x 4
(USB 3.0 x 1 for UTC-520D; USB 3.0 x 2 for UTC-520C/E)
H. HDMI Port
I. VGA Port
J. LAN Ports x 2
K. CFast Slot (UTC-520A/B only)
L. DC Input
M. Power Switch
A B D F H K M
L
G JIC E
I/O Ports UTC-500 Appearance
For more information on this and other Advantech
products, please visit our website at:
http://www.advantech.com
http://www.advantech.com/eplatform
For technical support and service, please visit our
support website at:
http://www.advantech.com/support
This manual is for the UTC-500 Series Rev.A1.
Part No. 2008050020
Printed in Taiwan
1st Edition,
September, 2014
Touch Panel &
LCD Display
VESA Mounting
I/O Ports
Side Groove
A B C D E F G H I J
K
L M
2 UTC-500 Series Startup Manual
UTC-532:
A. Power Switch
B. USB 2.0 x 4
(USB 3.0 x 1 for UTC-532D; USB 3.0 x 2 for UTC-532C/E)
C. HDMI Port
D. VGA Port
E. LAN Ports x 2
F. Antenna Port
G. Line-out
H. Mic-in
I. COM3 (UTC-532A only)
J. COM2
K. COM1
L. AC input
Manufacturer:
Advantech Co., Ltd. No.1, Alley 20, Lane 26, Rueiguang
Road Neihu District, Taipei, Taiwan 114, R.O.C. TEL: (02)
2792-7818
Distributed in Europe by:
Advantech Europe GmbH Kolberger Straße 7 D-40599
Düsseldorf, Germany
Tel: 49-211-97477350
Fax: 49-211-97477300
Power On Computer:
1. Connect an adaptor with input voltage rated 12V/5A for
all UTC-515 and UTC-520A/B/D SKUs.
2. Connect an adaptor with Input voltage rated 12V/7A for
UTC-520C/E SKUs.
3. Connect an AC power cable for all UTC-532 SKUs
(100-240VAC, 50/60 Hz).
4. Be sure always handle the power cords by holding the
plugs ends only. Please refer to I/O Ports section above
to find the DC/AC inlet and power switch.
5. Press Power On/Off. The PWR LED will turn green
Install Optional Modules:
1. Attach the UTC-peripheral to the side groove.
2. Fasten the 2 screws to fix the peripheral in place.
3. Connect the cable to an I/O port (USB).
4. Choose a location to place cable clamp and attach
cable to it for simplify cable routing
Please read these safety instructions carefully and strictly
follow these instructions for use. Repair of the device may
only be carried out by trained service personnel. Advantech
recommends that a service contract be obtained with
Advantech service and that all repairs also be carried out by
them; otherwise the correct functioning of the device may
be compromised.
WARNING! Because of the danger of electric shock, never
remove the cover of a device while it is in opera-
tion or connected to a power outlet.
If one of the following situations arises, have the equipment
checked by service personnel:
• The power cord or plug is damaged.
• Liquid has penetrated the equipment.
• The equipment has been exposed to moisture.
• The equipment does not work well, or you cannot get it to
work according to the user’s manual.
• The equipment has been dropped and damaged.
• The equipment has obvious signs of breakage. Discon-
nect this equipment from any AC outlet before cleaning.
Use a damp cloth. Do not use liquid or spray detergents
for cleaning and keep this equipment away from humidity.
CAUTION! To avoid short-circuits and otherwise damaging
the device, do not allow fluids to come in contact
with the device. If fluids are accidentally spilled
on the equipment, remove the affected unit from
service as soon as possible and contact service
personnel to verify that patient safety is not com-
promised.
If your computer clock is unable to keep accurate
time or the BIOS configuration resets to default,
please check the battery.
CAUTION! Do not replace the battery yourself. Please con-
tact a qualified technician or your retailer.
The computer is provided with a battery-powered
real-time clock circuit. There is a danger of explo-
sion if battery is incorrectly replaced. Replace
only with same or equivalent type recommended
by the manufacturer. Discard used batteries ac-
cording to the manufacturer’s instructions.
I/O Ports (cont.) Safety Instructions
A B E F G H I J K LC D
Easy Setup

Products related to this Datasheet

15.6" PCT.T/S PANEL WITH AMD T40
Available Quantity: 0
Unit Price: 0
15.6" RES.T/S PANEL WITH AMD T40
Available Quantity: 0
Unit Price: 0
15.6" PCT.T/S PANEL WITH ATOM D2
Available Quantity: 0
Unit Price: 0
15.6" RES.T/S PANEL WITH ATOM D2
Available Quantity: 0
Unit Price: 0
15.6" PCT.T/S PANEL WITH INTEL C
Available Quantity: 0
Unit Price: 0
15.6" RES.T/S PANEL WITH INTEL C
Available Quantity: 0
Unit Price: 0
21.5 UTC WITH AMD T40E/2G MEMORY
Available Quantity: 0
Unit Price: 0
21.5" PCT.T/S PANEL WITH AMD T40
Available Quantity: 0
Unit Price: 0
LCD DISPLAY 21.5" RES T/S PANEL
Available Quantity: 0
Unit Price: 0
21.5" PCT.T/S PANEL WITH ATOM D2
Available Quantity: 0
Unit Price: 0
21.5" PCT.T/S PANEL WITH I7 3517
Available Quantity: 0
Unit Price: 0
LCD DISPLAY 21.5" RES T/S PANEL
Available Quantity: 0
Unit Price: 0
21.5" UTC WITH BAYTRAIL J1900/ 4
Available Quantity: 0
Unit Price: 0
21.5" RES.T/S PANEL WITH BAYTRAI
Available Quantity: 0
Unit Price: 1347.33
21.5" UTC WITH HASWELL I5-4300U
Available Quantity: 0
Unit Price: 0
32" UTC WITH AMD T40E / 4G MEMOR
Available Quantity: 0
Unit Price: 0
32" PCT.T/S PANEL WITH I7 3517UE
Available Quantity: 0
Unit Price: 0
32" PCT.T/S PANEL WITH BAYTRAIL
Available Quantity: 0
Unit Price: 3148.7
32" UTC WITH HASWELL I5-4300U/ 4
Available Quantity: 0
Unit Price: 0
32" PCT.T/S PANEL HASWELL I5-43
Available Quantity: 0
Unit Price: 3680.64