Effective Thermal Management of LED Arrays

Por Bridgelux, Inc.

Colaboración de Convergence Promotions LLC


The performance, reliability, and design life of LED arrays depend heavily on proper thermal management. This article examines a variety of conduction, convection, and radiation techniques to help ensure optimal performance and long life for your next lighting design.

Introduction

The Bridgelux family of LED Array products delivers high performance, compact, and cost-effective solid-state lighting solutions to serve the general lighting market. These products combine the higher efficiency, lifetime, and reliability benefits of LEDs with the light output levels of many conventional lighting sources.

As noted in Bridgelux LED Array product datasheets, several performance characteristics of the LED Array products, including flux, forward voltage, color, and reliability are dependent upon temperature. This is a common characteristic for all LEDs, a characteristic of the semiconductor-based technology. As temperature increases, several performance parameters experience a temporary and recoverable shift. With increasing temperature, light output (or flux) decreases, forward voltage (or Vf) decreases, and the color temperature shifts towards blue.

Furthermore, absolute maximum ratings, such as maximum case temperature and maximum junction temperature, must not be exceeded. Exceeding the absolute maximum ratings, as listed in the product datasheets, may irreversibly damage the product and cause permanent shifts in performance.

Optimization of performance and reliability in a lighting system using Bridgelux LED Arrays requires proper thermal management. Although a critical design parameter, thermal management is not as difficult as many would believe. Understanding the basics allows every lighting designer to optimize his product and meet specification requirements.

This article describes basic thermal management concepts and guidelines for proper use of Bridgelux LED Arrays in a lighting system. Included is an overview of basic heat transfer concepts, a description of a thermal model, a sample calculation using this thermal model, a description of various thermal components, and recommendations for measuring the case temperature of the Bridgelux LED Array to validate the performance of the thermal management solution.

Photo


Heat generation

When voltage is applied across the junction of an LED, current flows through the junction generating light. It is a common misconception that LEDs do not generate heat. While essentially no heat is generated in the light beam (unlike conventional light sources), heat is generated at the case of the LED Array and must be effectively managed. As LEDs are not 100 percent efficient at converting input power to light, some of the energy is converted into heat and must be transferred to the ambient. The amount of heat generated from the LED Array that must be transferred to the ambient may be conservatively estimated to be the power that is applied to the LED Array, or Pd, and may be calculated by multiplying the forward voltage (Vf) times the current (If). This is described in Equation 1.

Equation

Equation 1: Power Dissipated

Where:
  Pd is the thermal power dissipated
  Vf is the forward voltage of the device
  If is the current flowing through the device

The maximum dissipated power for each of the Bridgelux LED Array products is listed in Table 3 of this article. It should be noted that any input power (Vf * If) that is converted to light is usually ignored when calculating the total thermal load. Ignoring the devices thermal efficiency provides a safety margin in the design of the thermal solution.

Heat generated by additional sources, such as a power supply located near the LED Array, must also be managed. In order to reduce the size and cost of the thermal management solution and to minimize the amount of additional heat added to the system, power supplies and other heat generating components should not be located in close proximity to the LED Array.

Thermal path

Heat generated at the LED junction must be transferred to the ambient via all elements that make up the thermal management solution. These elements include the LED Array, the thermal interface material used between the LED Array and heat sink, the heat sink, the luminaire enclosure (if applicable), and other components that come in contact with the lighting assembly. These elements transfer heat to the ambient through conduction, convection, or radiation. These heat transfer modes will be discussed in greater detail in the next section of this application note. For a simple thermal management solution that consists of an LED Array mounted to a heat sink, we consider that all the heat from the LED junction is typically transferred to the ambient through the following thermal path:
  1. Heat is conducted from the semiconductor chip within the LED Array to the elements that make up the LED Array, including the metal board and the silicone resin.
  2. Heat is then conducted from the LED Array through a thermal interface material to the heat sink of the lighting system. This is a critical component in transferring the heat. We will discuss this point in detail later.
  3. Heat is then conducted through the heat sink.
  4. Heat is then convected to the air around the heat sink and is radiated to the ambient.
Modes of heat transfer

There are three basic modes of heat transfer; conduction, convection, and radiation. All heat flow is driven by temperature gradients; heat moves from hot to cold. Each heat transfer mode plays an important role in transferring heat away from the LED junction to the ambient. Table 1 provides a summary describing the various heat transfer modes and the equations that govern them.

The first of these, conduction, is the transfer of heat between adjacent molecules of a material, usually a solid. Equation 2 provides the basis for our first set of guidelines for designing meaningful thermal solutions.

Considerations for heat sink design or selection:
  • Minimize the distance heat must travel (dx). In practical terms, this means that if a heat sink is too large, it may lose effectiveness. However, this distance should not be so small that a bottleneck is created, constricting the flow of heat.
  • Select heat sinks made of materials that have a high thermal conductivity (k). As a reference, Table 2 compares thermal conductivity of various metals typically used for heat sinks and the thermal conductivity of air. Although aluminum is not as an effective heat conductor as copper, it is frequently the material of choice as it minimizes the cost and the weight of the thermal solution.
  • Use heat sinks with large surface areas (A).
  • Eliminate air gaps and voids between the LED Array and the heat sink. Air is a very poor conductor of heat. During assembly, the flat bottom surface of the LED Array should be in full contact with the flat surface of a heat sink. If air gaps or voids exist between the two, a thermal interface material should be used to fill the gaps.
Mode Governing Equation Definition of Variables
Conduction QCOND= -k A dT/dx
Equation 2: Heat Conduction
QCOND is the heat that is conducted (°C/Wm)
k is the thermal conductivity of the material (W/mK)
A is the cross sectional area of the medium the heat is conducted through (m2)
dT is the temperature gradient across the material (°C)
dx is the distance the heat is traveling through the material (m)
Convection QCOND= h A (Ts — T)
Equation 3: Heat Convection
QCOND is the heat convected
h is the convection heat transfer coefficiency (W/m2K)
A is surface area
Ts is the surface temperature of the hot surface
T is the temperature at infinity, typically the ambient air temperature
Radiation QRAD= εσ A (T4s — T4)
Equation 4: Heat Radiation of Gray Bodies*
QRAD is radiated heat
ε is emissivity and provides a measure for how a surface emits energy relative to a blackbody
σ is the Stephan-Boltzmann Constant, 5.6703 10-8 (W/m2K4
A is the area of the emitting body
Ts is the surface temperature
T is the temperature at infinity, typically the ambient air temperature

Table 1: Heat transfer modes and governing equations.

* In the real world, the ideal models of Physics do not absolutely apply. Typically, engineers assume that heat radiation does not depend on the sample’s surface conditions. In these cases, the heat source is known as a “Gray Body."

Nature has two great thermal insulators. The first great insulator is a vacuum, and the second is air. Therefore, it is critical to have a sufficient volume of the thermal interface material to displace the air. However, if there is any excess thermal interface material, for example more than 0.3mm, then the system thermal resistance will begin to increase. On the surface, this may not appear to make sense. What one needs to consider is that while the thermal interface material is better at removing heat than air, it is much worse than the metal in the heat sink that conducts the heat away from the LED Array.

Material Thermal Conductivity (W/mK)
Iron 79.5
Aluminum 205
Copper 385
Air (at 0°C) 0.024

Table 2: Thermal conductivity of common heat sink materials and air.

Convection describes heat transfer due to random molecular motion and bulk motion of a fluid. In other words, convection is the heat transfer from the heat sink to air (or water) and is directly dependent upon the amount of flow of the air or water. In the case of the natural convection in air, where, for example, the movement of air molecules in not aided by a fan, the convection heat transfer coefficient ranges from 2 to 15 W/m2K.

Forced convection is a result of movement in the fluid (water or air), which results from other forces, such as the use of a fan or pump. With forced convection, the convection heat transfer coefficients range from 25 to 250 for gases and from 100 to 20,000 for liquids. Both natural convection and forced convection may be used to effectively convect heat away from the LED Array. Equation 3 can be used to develop guidelines for enabling heat transfer through convection.

Considerations for heat sink design or selection:
  • Use heat sinks with the largest surface area (A) that is physically or economically feasible. As a general rule of thumb, for a well-ventilated heat sink, there should be 10 square inches of heat sink for every 1 watt of power dissipated. The use of pinned heat sinks, however, is not recommended.
  • Orient heat sink fins in a manner that allows hot air to flow upward and away from the heat sink and cold air to flow onto the surfaces of the heat sink.
  • Avoid constricting the airflow.
  • If possible, use natural convection to transfer heat from the heat sink to the ambient. Doing so avoids potential reliability issues of fans.
  • If natural convection is insufficient, then consider using fans, heat pumps, or liquid cooling elements that can dramatically increase the convection heat transfer coefficient and hence dramatically increase heat transfer.
  • Use heat sinks with surfaces that have high emissivity values.
  • Radiation is energy transfer by electromagnetic waves. By analyzing Equation 4, guidelines for enabling heat transfer through radiation can be developed.
  • Radiation heat transfer has a very strong dependency on temperature. The hotter the heats sink, the more significant the heat transfer through radiation. However, as the maximum case temperature of the LED Array is 105°C, heat transfer due to radiation is very small when compared to other heat transfer modes.
Keeping in mind how heat is transferred and consciously optimizing specific heat transfer modes should make the task of designing a cost effective and optimally sized thermal management solution easier. In a typical single LED Array lighting assembly using simple heat sinks, the amount of heat that is conducted, convected, and radiated is a function of the heat sink geometry, surface area, material properties, surface properties, fin geometry (including thickness and spacing), and heat sink temperature. While this may sound complicated, the application of effective heat sink design is straightforward.

Thermal model

A simple thermal model or thermal circuit can illustrate the heat flowing through an LED Array. This model is analogous to an electrical circuit where heat flow is represented by current, voltages represent temperatures, heat sources are represented by constant current sources, and resistors represent thermal resistances. Figure 1 shows a thermal circuit for a single LED Array mounted to a heat sink.

Simple thermal circuit

Figure 1: Simple thermal circuit

Where:
  Q is heat flowing from hot to cold through the LED
  Tj is the temperature at the junction of the device
  Tc is the temperature at the case of the LED Array
  Th is the temperature at the point where the heat sink is attached to the LED Array
  Tamb is the ambient air temperature
  jc is the thermal resistance from junction to case of the LED Array
  ch is the thermal resistance between the case of the LED Array and the heat sink
  ha is the thermal resistance of the heat sink

With the exception of Tj, all temperatures listed above can be easily measured. For Bridgelux LED Arrays, case temperature measurements are made in the area noted in the mechanical drawings section of the product datasheets. Note that this area is on the same surface of the LED Array as the resin area, providing an easy to measure location after assembly to the heat sink. Although traditionally case temperature measurements are conducted on the back side of device, the difference in temperature between the defined case temperature measurement point location on the top of the Bridgelux LED Array and bottom are very small. Bridgelux has characterized the difference between these two points to be typically 1°C or less and considers the difference negligible.

The thermal resistances that make up the thermal model may be calculated and solved for using the following equation:

Equation

Equation 5: Thermal Resistance

Where:
  xy is the thermal resistance from x to y, where x and y are points along the thermal circuit
  Tx is the temperature at x
  Ty is the temperature at y
  Q is heat flow and may be approximated to be Pd (see Equation 1)

Substituting “x” with “j” and “y” with “c,” we get Rθjc, or the thermal resistance from junction to case of the LED Array. Rθjc values are included in the Product Data Sheets for all Bridgelux LED Arrays and therefore do not need to be calculated. Instead, by knowing Rθjc values and by using Equation 5, we may solve for Tj, the temperature at the junction.

By substituting “x” and “y” with appropriate values, both Rθch and Rθha may be solved for using Equation 5. When using thermal interface materials, such as thermal pastes and adhesives, Rθch describes the thermal resistance of the thermal interface material. Thermal interface materials and their impact on thermal resistance will be discussed in greater detail later in this article. Rθha describes the thermal resistance of a heat sink or heat sink assembly. Once maximum operating conditions are known, including drive current, forward voltage, and maximum ambient temperature, this value is solved for, and a heat sink may be sized and selected to achieve this value.

Rules governing a thermal circuit are also analogous to those of an electric circuit. Equation 6 depicts the method for adding series thermal resistance values.

Equation

Equation 6: Summation of series thermal resistances.

Where Rθja is typically referred to as the system thermal resistance.

Furthermore, when assembling multiple LED Arrays on a single heat sink, the rule of parallels applies. This is depicted in Equation 7.

Equation

Equation 7: Summation of parallel thermal resistances.

In Equation 7, “n” refers to the number of LED Arrays mounted onto a single heat sink and Rθn jh is the thermal resistance from the LED junction to the heat sink of each of the individual LED Arrays. It should be noted that when using this model the total power (sum of all LED Arrays mounted to the single heat sink) must be multiplied by the system thermal resistance to calculate the case or junction temperature.

Thermal Model Example

Design Challenge:

A luminaire is to be designed using the BXRA-C1202-00000 LED Array driven at 1050 mA. The maximum ambient temperature will be 40°C and the case temperature cannot exceed 70°C in the application. A thermal paste, with a thermal conductivity of 4 W/mK and a resulting thermal resistance of 0.07 vC per watt has been selected. Shifts in forward voltage due to temperature are assumed negligible. Given this information, the thermal resistance of the heat sink required for this design must be calculated and the minimum surface area for an extruded aluminum heat sink must be determined.

Simple thermal circuit

Figure 2: Simple thermal circuit of multiple LED Arrays on a single heat sink.


Photo
Solution:

To solve for the thermal resistance of the heat sink, we use equation 5, where “x” is “h” and “y” is “a”:

Equation

Here, Ta is 40°C and Th is unknown at this time, but may be solved for. Q is the dissipated power, which is the product of the voltage and current. In order to design a thermal management system to account for the entire range of product performance, the maximum forward voltage of the LED Array must be used (see Table 3 or the relevant product datasheet).

Equation

As the thermal resistance of the thermal interface material is known, to solve for Th we use equation 5, substituting “x” with “c” and “y” with “h”:
Equation


Equation

Now solving for Rθha :
Equation

The surface area of a black anodized aluminum extruded heat sink with at thermal resistance of 2°C/W is estimated to be at least 101.5 square inches for a heat sink with fins that are oriented vertically or 145 square inches if the fins are oriented non-vertically. While these values may appear large, this is the total surface area required and may consist of surfaces that make up the luminaire itself such as the housing and reflector, in addition to the surfaces that make-up the heat sink. The final required surface area of the heat sink depends on many variables, including, but not limited to, fin orientation, the ability of hot air to move away from the heat sink, the ability of cold air to enter and flow through the heat sink, and the existence of other heat sources near the LED Array.

Thermal solution components — heat sinks

There are many commercially available components, including heat sinks and heat pipes, which may be used with Bridgelux LED Arrays. The most commonly used components are heat sinks, typically made of aluminum or copper. Heat sinks conduct heat from a heat source and then convect the heat to the ambient. The size of a required heat sink depends on many variables, including the temperature requirements for the application (such as maximum ambient and case temperature), the material of the heat sink, the surface characteristics of the heat sink, and the physical constraints for the application.

Table 3 lists minimum surface areas and sample dimensions for reference heat sinks in simple cases where a single LED Array is used in a light fixture, and natural convection and radiation are used to transfer heat to the ambient. Calculated thermal resistance values of the reference heat sinks (Rha) in Table 3 are based on the following:
  • The maximum ambient temperature of the application is 40°C.
  • The maximum case temperature of the array is 70°C.
  • The thermal interface material used has a thermal conductivity of 4W m/K (like that of Dow Corning TC-5022). The thermal resistance contributions for various thermal interface materials are shown in Table 5. These values vary by LED Array product and range from 0.19°C/W for the LS Array Series products to 0.035°C/W for the RS Array Series products.
  • Maximum dissipated power values have been calculated using forward voltage values reached at elevated junction temperatures, those reached when the LED Arrays reach a case temperature of 70°C.
The surface area and dimension values listed in Table 3 are based on the reference heat sink (Rha) values.

Table 3 illustrates that when relying on natural convection to transfer heat to the ambient, the minimum required surface area for an extruded aluminum heat sink with a black anodized finish is 10 in2 per watt of dissipated power. This area may be provided as a flat plate or via a finned extruded heat sink to minimize the volume of the thermal management solution. The required heat sink surface area must be determined and validated by the luminaire designer and will depend on many luminaire design variables, including fin orientation and cold and hot air flow paths.

In some applications, space requirements may not allow for such a large heat sink. In these cases, designers should consider using forced convection elements, such as fans. Consult heat sink suppliers to explore forced convection heat sink options. Heat sink suppliers can provide detailed technical data on their heat sinks to customers. Data supplied includes heat sink temperature rise above ambient as a function of air flow speed and heat sink thermal resistance as a function of air flow speed. This information aids in the design and heat sink selection process.

Part Number Electrical Characteristics Reference Heat Sink Characteristics With Free Convection
Maximum Voltage at Tj=25°C (V) Maximum Voltage at Tcase=70°C (V) Current (mA) Power(W) Rha (°C/W) Surface Area (in2) Surface Area (mm2) Dimensions (mm3)
Warm White BXRA-W0240 14.3 13.9 350 4.9 6.15 48.8 31477 38.1x16x84
BXRA-W0241 7.3 7.1 700 5.0 6.02 49.8 32155 39.6x19x105
BXRA-W0260 13.6 13.2 350 4.6 6.47 46.3 29897 38.1x16x84
BXRA-W0261 6.8 6.6 700 4.6 6.47 46.3 29897 38.1x16x84
BXRA-W0400 10.6 10.3 900 9.3 3.23 93.0 59981 88.9x21.6x84
BXRA-W0401 10.3 10.0 700 7.0 4.27 70.2 45297 57.1x20.6x91
BXRA-W0402 9.7 9.4 700 6.6 4.54 66.0 42587 57.1x20.6x91
BXRA-W0403 31.7 30.9 250 7.7 3.88 77.2 49822 50.4x25x105
BXRA-W0800 14.3 13.9 1300 18.1 1.66 181.2 116916 73.3x25.4x91
BXRA-W0802 13.2 12.8 1050 13.5 2.23 134.8 86980 76.1x57.1x91
BXRA-W1200 17.8 17.4 1600 27.8 1.08 277.6 179096 100x40x210
BXRA-W1202 16.3 15.9 1200 19.0 1.58 190.2 122709 73.3x25.4x91
BXRA-W1203 19.8 19.3 1050 20.2 1.48 202.2 130471 66x40x210
BXRA-W3000 28.3 27.6 2100 57.9 0.52 579.2 373664 160x40x308

Table 3a: Critical parameters and sample heat sink dimensions for Warm White LED Arrays by part number.

Part Number Electrical Characteristics Reference Heat Sink Characteristics With Free Convection
Maximum Voltage at Tj=25°C (V) Maximum Voltage at Tcase=70°C (V) Current (mA) Power(W) Rha (°C/W) Surface Area (in2) Surface Area (mm2) Dimensions (mm3)
Neutral White BXRA-N0400 10.5 10.2 800 8.2 3.67 81.8 52800 57.1x20.6x140
BXRA-N0402 9.7 9.4 600 5.7 5.30 56.6 36503 32.5x25x42
BXRA-N0800 14.1 13.7 1200 16.5 1.82 164.9 106374 73.3x25.4x91
BXRA-N0802 13.2 12.8 1050 13.5 2.23 134.8 86980 76.2x38.1x140
BXRA-N1200 17.5 17.1 1400 23.9 1.26 238.7 154000 80x40x280
BXRA-N1203 19.8 19.3 1050 20.2 1.48 202.2 130471 66x40x210
BXRA-N3500 28.3 27.6 2100 57.9 0.52 579.2 373664 160x40x308

Table 3b: Critical parameters and sample heat sink dimensions for Neutral White LED Arrays by part number.

Impact of fin orientation on heat sink performance

Thermal performance presented by heat sink manufacturers usually pertains to the most favorable heat sink orientation, which is with the fins of the heat sink oriented vertically (see Table 4). In this orientation, hot air rises readily, allowing cool air to circulate through the fins. Other orientations give varying results. Rules of thumb on the impact of varying fin orientation are shown in Table 4. However, please note that the actual performance of a heat sink is dependent upon many variables such as heat sink location within an assembly, the location of other heat generating elements such as a power supply, effective airflow, fin spacing, fin height, fin thickness, base thickness, base surface area, shape, fin geometry, and overall length. Consequently, the effectiveness of a heat sink mounted in varying orientations is not a fixed number, and depends on the inter-relationship between many variables. A much larger poorly positioned heat sink will not be as effective as a properly oriented thermal system.

Part Number Electrical Characteristics Reference Heat Sink Characteristics With Free Convection
Maximum Voltage at Tj=25°C (V) Maximum Voltage at Tcase=70°C (V) Current (mA) Power(W) Rha (°C/W) Surface Area (in2) Surface Area (mm2) Dimensions (mm3)
Cool White BXRA-C0360 14.3 13.9 350 4.9 6.15 48.8 31477 38.1x16x84
BXRA-C0361 7.3 7.1 700 5.0 6.02 49.8 32155 39.6x19x105
BXRA-C0400 10.6 10.3 600 6.2 4.84 62.0 39987 53.3x11.8x140
BXRA-C0402 10.3 10.0 500 5.0 5.98 50.2 32355 39.6x19x105
BXRA-C0603 31.7 30.9 250 7.7 3.88 77.2 49822 57.1x20.6x140
BXRA-C0800 14.1 13.7 900 12.4 2.43 123.7 79780 76.2x38.1x140
BXRA-C0802 13.7 13.3 700 9.3 3.21 93.4 60245 88.9x21.6x84
BXRA-C1200 14.3 13.9 1300 18.1 1.66 181.2 116916 73.3x25.4x91
BXRA-C1202 13.8 13.4 1050 14.1 2.13 141.1 91045 76.1x57.1x91
BXRA-C2000 18.0 17.7 1750 31.0 0.97 310.3 200177 100x40x210
BXRA-C2002 17.5 17.1 1500 25.6 1.17 255.8 165000 80x40x280
BXRA-C4500 28.3 27.6 2100 57.9 0.52 579.2 373664 160x40x308

Table 3c: Critical parameters and sample heat sink dimensions for Cool White LED Arrays by part number.

To illustrate the effect of fin orientation and limiting airflow, measurements of case temperature and heat sink temperature of a BXRA-C1200 LED Array were conducted. The LED Array was mounted to a 121 x 121 x 32 mm heat sink with a surface area of 774 cm2. A thin layer of thermal paste was applied between the LED Array and the heat sink. The dissipated power for this LED Array was 18.4 watts. The heat sink was then placed in the orientations listed in Table 4. When sitting on a flat surface, the heat sink sat on a 1-inch thick foam board to minimize conduction to the bottom surface. Measurements were taken after one hour of operation in each configuration.

Some results vary from the guidelines listed in Table 4, illustrating the need to measure a proposed or calculated design to gauge true effectiveness of a thermal management solution. There may be many variables that cause differences in results, such as uncontrolled forced convection from central heating units and differing amounts of heat conduction to surroundings. All must be taken into consideration when designing a thermal solution.

Note that the worst performance was achieved by placing the LED Array in a box and limiting both conduction and natural convection airflow paths. The thermal resistance of the system could be significantly improved in this case by providing a convective path to ambient. Typically LED-based luminaires are constructed in such a manner as to conduct the heat to the exterior case of the luminaire, significantly improving the thermal performance of the system.

As mentioned previously, fans may be used to dramatically increase the convection heat transfer coefficient and hence dramatically increase heat transfer from the heat sink to the ambient. If fans are used, make sure that they pull in the cold ambient air to the heat sink surfaces and that they push hot air away from the heat sink. Also, make sure the lifetime of any active thermal management system is evaluated to ensure it is suitable, matching, or exceeding the expected life of the lighting assembly.

Fin Orientation Illustration Guideline Experimental Results
Typical Relative Effectiveness Measured Th ha (°C/W) Typical Relative Effectiveness
Vertical Photo 100% 65°C 2.2 100%
Horizontal Photo 85% 69°C 2.5 88%
Horizontal Up Photo 70% 84°C 3.2 61%
Horizontal Down Photo 60% 66°C 2.3 83%
Vertical (inside a 6 x 7 x 7 in3 Non-Conducting Box) Photo 95°C 3.9 27%

Table 4: Impact of heat sink fin orientation on heat sink effectiveness, general rules, and experimental results.

Thermal interface management

To ensure heat flow from the LED Array to a heat sink, pay close attention to air gaps or voids located between the bottom of the LED Array and the heat sink. Such voids will significantly impede the flow of heat and therefore must be eliminated. The use of thermal interface materials, such as thermal greases, pastes, or adhesives, is recommended to ensure that air gaps and voids are eliminated.

When selecting a thermal interface material, many factors must be considered. These include thermal conductivity, operating temperature range, cost, workability (dispensability for pastes), electrical conduction, and the ability to control the thickness of the bond line. If using a paste, the amount of paste that is dispensed should be enough to cover the entire base of the LED Array, but not so much as to result in a thick bond line, which will increase the thermal resistance. Application of excess thermal interface material can also create side fillets. Fillet size should be kept at a minimum and must not touch the top of the LED Array.

The following equation shows the relationship between thermal interface material thickness and thermal resistance:

Equation

Equation 8: Thermal resistance of an interface material.

Where:
  L is the thermal interface material thickness (mm)
  K is the thermal conductivity (W/m-K)
  Ac is the contact area (mm2)

For design purposes, the thermal interface material thickness typically ranges from 0.15 to 0.30 mm, depending on the LED Array product and the thermal interface material selected. This range of thicknesses assumes that the planarity of the bottom surface of the LED Array is maintained at or below 0.1 mm for all products except RS Array Series products. The planarity for the RS Array Series products is maintained at or below 0.25 mm. Hence, when selecting a thermal interface material ensure that the thickness of the material is sufficient to fill gaps between the base of the LED Array and the heat sink while at the same time minimizing the thickness. Thermal conductivities of interface materials vary from product to product. Table 5 lists a few examples and the impact on the thermal resistance of a lighting system for various Bridgelux LED Array products.

Part Numbers Thermal Interface Material Product Thermal Conductivity (W/mK) Thickness (mm)[1] Estimated Interface Resistance[2] (°C/W)
BXRA-W0240
BXRA-W0241
BXRA-W0260
BXRA-W0261
BXRA-C0360
BXRA-C0361
Aavid Thermalloy Sil Free 1020 0.79 0.15 0.96
Berquist A1500 2 0.254 0.64
Chomerics T777 2.2 0.15 0.34
Omega OT-201 2.24 0.15 0.34
Laird Tgrease 2500 3.8 0.15 0.20
Dow Coming TC-5022 4 0.15 0.19
BXRA-W0400
BXRA-W0401
BXRA-W0402
BXRA-W0403
BXRA-N0400
BXRA-N0402
BXRA-C0400
BXRA-C0402
BXRA-C0603
Aavid Thermalloy Sil Free 1020 0.79 0.15 0.63
Berquist A1500 2 0.254 0.42
Chomerics T777 2.2 0.15 0.23
Omega OT-201 2.24 0.15 0.22
Laird Tgrease 2500 3.8 0.15 0.13
Dow Coming TC-5022 4 0.15 0.12
BXRA-W0800
BXRA-W0802
BXRA-N0800
BXRA-N0802
BXRA-C0800
BXRA-C0802
BXRA-W1200
BXRA-W1202
BXRA-W1203
BXRA-N1200
BXRA-N1203
BXRA-C1200
BXRA-C1202
BXRA-C2000
BXRA-C2002
Aavid Thermalloy Sil Free 1020 0.79 0.15 0.34
Berquist A1500 2 0.254 0.22
Chomerics T777 2.2 0.15 0.12
Omega OT-201 2.24 0.15 0.12
Laird Tgrease 2500 3.8 0.15 0.07
Dow Coming TC-5022 4 0.15 0.07
BXRA-W3000
BXRA-N3500
BXRA-C4500
Aavid Thermalloy Sil Free 1020 0.79 0.3 0.176
Berquist A1500 2 0.254 0.059
Omega OT-201 2.24 0.3 0.062
Laird Tgrease 2500 3.8 0.3 0.036
Dow Coming TC-5022 4 0.3 0.035

Table 5: Thermal conductivity and estimated thermal resistance of some thermal interface materials.
  1. For all products except RS Array series products, flatness of the back surface of the LED Array is maintained at < 0.1 mm across the LED Array. For RS Array Series products, flatness is maintained at < 0.25 mm across the LED Array. Examples shown assume this worst-case scenario.
  2. Thermal interface material thickness is assumed to be 0.05 mm for all materials except the Berquist A1500 Sil-Pad. The Berquist A1500 Sil-Pad is 0.254 mm thick.
All thermal interface materials must be applied in a way that ensures the entire bottom of the LED Array is covered and that air gaps or voids between the LED Array and the heat sink are filled. One method of achieving this, which may be used in volume production, is to silkscreen precise quantities of a dispensable thermal interface material on a heat sink surface prior to attaching the LED Array.

Silkscreen templates are made in sizes that mirror the base of the LED Array or are scaled to a slightly larger size. The final thickness of the interface material is controlled by the force applied on the LED Array from the top when pressing it down on the thermal interface material. These forces can vary from a few hundred grams, which pick and place equipment is capable of handling, to several kilograms, which would require special tooling. If pick and place equipment is used for this processes, consider using “Scrub” mode, while pressing the LED Array onto the heat sink. In all cases, care must be taken to avoid contact with the resin area of the LED Array during assembly. Please consult application note AN11 — Handling and Assembly of Bridgelux LED Arrays, for further information.

The customer must evaluate the performance of the thermal interface material to ensure adequacy in terms of thermal performance, manufacturability, and durability.

Use of current derating curves

Current derating curves are included in the Bridgelux LED Array Product Data Sheets. These curves provide guidance to customers in developing effective thermal management solutions that meet system design requirements.

A derating curve is included for each Bridgelux LED Array product. When using these graphs, the required system thermal resistance can be estimated when the LED Array is used at the rated test current under various ambient conditions. An example of one of these derating curves is included in Figure 3. Please consult the relevant product datasheets for the most recent versions of these derating curves.

Derating Curve
Figure 3: Derating curve for BXRA-W0400, 900 mA drive current.

The thermal resistance values indicated on the derating curves are total system thermal resistance values (junction to ambient). Although limited options are included, it is possible to interpolate between these curves for approximation purposes. The safest approach, however, is to calculate the required system thermal resistance using the equations contained in this application note.

The thermal resistance for the BXRA-W0400 product from the Bridgelux LED Array product datasheet is listed as 1.0°C/W. If in a given lighting system the thermal resistance from case to ambient is designed to deliver 3°C/W, the curve in Figure 3 labeled 4°C/W would be applicable for this lighting system (sum of junction to case and case to ambient thermal resistance values).

In this example, as long as the ambient temperature is maintained below 80°C, the maximum temperature ratings of the product will not be violated at the rated forward current of 900 mA. If, however, the ambient temperature was to rise to 85°C, the forward current would need to be reduced to 700 mA based on the 4°C/W system thermal resistance. Alternatively, a heat sink could be designed to deliver a case-to-ambient thermal resistance of 2°C/W. This would result in a system thermal resistance of 3°C/W, allowing for 900 mA operation at the 85°C ambient condition.

Measuring effectiveness of a thermal solution

After a thermal management solution has been designed, it is critical to experimentally validate the effectiveness of the solution. This is typically done by building a prototype, simulating the worst case use conditions, and measuring Tcase. When simulating worst case use conditions ensure the following:
  • Convection conditions are realistic.
  • Material properties and dimensions, including wall thicknesses, surface areas, and component sizes are representative of the design.
  • Surface properties, including color and roughness properties, are representative of the design.
  • Additional heat sources that may impact the thermal performance of the device are included (such as a power supply that is placed inside a luminaire enclosure or imbedded into a heat sink).
Once the representative prototype is built, and realistic use conditions are simulated, Tcase may be measured to validate the design.

Special care is required when measuring the case temperature to ensure an accurate measurement. The following approach is recommended to minimize measurement errors for attaching the thermocouple to the case temperature measurement point of the LED Array:
  • Use 36 gauge or smaller diameter K-type thermocouples.
  • Ensure that the thermocouple is properly calibrated.
  • Attach the thermocouple bead, or junction, to the area on top of the LED Array in the prescribed area (refer to the mechanical drawings section in the relevant product datasheet).
  • Attach the thermocouple to the LED Array using an adhesive that has high thermal conductivity. To do this, first place the thermocouple bead on to the prescribed area. Temporarily secure the thermocouple using Kapton tape. Next, using the back of a thin diameter wood stick, such as a tooth pick or the wooden end of a cotton swab, press on the thermocouple bead, ensuring contact with the LED Array board. Lastly, apply a small amount of a fast curing, low viscosity, and thermally conductive adhesive around the base of the thermocouple bead. Allow the adhesive to cure. Remove as much as the wooden stick as possible.
  • Note that it is critical that the entire thermocouple bead be secured tightly against the case. There should be no air gaps between the thermocouple tip and the case of the LED Array.
After turning on the LED Array, Tcase will increase with time as the assembly heats up. Eventually, the lighting assembly should reach a steady state temperature. The time required to reach a steady state temperature depends on the time-constant of the assembly, but is likely to be in the range of 45 minutes to an hour. Maintain the Bridgelux LED Array Tcase at or below the maximum case temperatures listed in the product datasheet to ensure functionality and reliability.

Convergence Logo

Descargo de responsabilidad: Las opiniones, creencias y puntos de vista expresados por los autores o participantes del foro de este sitio web no reflejan necesariamente las opiniones, las creencias y los puntos de vista de DigiKey o de las políticas oficiales de DigiKey.

Acerca de este autor

Bridgelux, Inc.

Acerca de este editor

Convergence Promotions LLC