Bill of Materials (BOM) Manager


Scheme It BOM (Bill of Materials) keeps track of part attributes including: RefDes, Name, Value, Manufacturer, Part Number, DigiKey Part Number, Description, and Notes.

BOM_table

Adding Parts to the BOM

Whenever a new schematic symbol is placed into a project, it automatically gets added to the BOM.

Editing Part Attributes

Edit the attributes in the BOM by clicking on a table cell. This changes the cell into an editable text area and allows you to input a value using your keyboard. Once you add or change a value, press the Enter key to complete the edit.

Sorting by Attribute

Change the sort order of the BOM table by clicking on an attribute in the table header.

Searching

Users may search in the BOM table to filter parts they need. All fields in the BOM are searchable. Searches in the BOM are case-insensitive.

Exporting BOM

You can export the BOM to a spreadsheet which can be used in DigiKey's Enhanced BOM Manager (https://www.digikey.com/en/resources/bom-manager). This allows you to make further edits to your BOM and manage your components.

Import BOM

Scheme It also allows you to import your BOM to your current project by selecting the "click to import" option under the "Import BOM" category of the left sidebar. On the Imported BOM, the symbol components loaded can be assigned, removed, or deleted.

Request Quote

Send a quote request to DigiKey for the price and availability of your BOM by clicking on the "Quote" button under the BOM tab.

Order Parts

You can order parts in the BOM with "Order" button. Only parts with valid DigiKey Part Number are eligible. For symbols having no part number, if you want to assign a part number for them, use Catalog Assign feature.

BOM and MyLists

Part numbers used in the schematic are summarized in the BOM (Bill of Materials) tab.

You can create a DigiKey myLists from BOM tab.

DigiKey myLists let you access pricing, availability, lead times, and more.

In the BOM tab, you can download the list of part numbers for offline use (.xls file) or buy those parts from DigiKey.