6000 Series Cartridge User Instr Datasheet by 3M

View All Related Products | Download PDF Datasheet
1
Cartridge 6000 Series
User Instructions for 3M™ Cartridge 6001(07046), 6002,
6003(07047), 6004, 6005, 6006, and 6009
Important: Keep these User Instructions for reference.
For use only with 3M™ 6000 Series, 7000 Series and FF-400 Series half and full facepiece
respirators according to the NIOSH approval label.
07046 and 07047 are catalog numbers only. NIOSH approved as 3M™ 6001 Organic Vapor
Cartridge and 6003 Organic Vapor/Acid Gas Cartridge.
E
2
These cartridges help protect against certain airborne contaminants. Misuse may result
in sickness or death. For proper use, see supervisor, or User Instructions, or call 3M in
U.S.A., 1-800-243-4630. In Canada, call Technical Service at 1-800-267-4414.
Use cartridge before expiration date.
IMPORTANT
Before use, the wearer must read and understand these User Instructions, and the User Instructions
for the 6000 Series, 7000 Series or FF-400 Series half or full facepiece respirator to be used with
these cartridges. Keep these User Instructions for reference.
Use For
Respiratory protection from certain airborne contaminants according to NIOSH approvals, OSHA
limitations, in Canada CSA standard Z94.4 requirements, other applicable regulations and 3M
instructions. For additional information on 3M use recommendations please consult the 3M
Respirator Selection Guide found on the 3M OH&ESD website at www.3M.com/OccSafety or call
1-800-243-4630 in U.S.A. In Canada call 1-800-267-4414.
Do Not Use For
- Particulates, unless combined with approved particulate filters.
- Sandblasting
Use Instructions
1. Failure to follow all instructions and limitations on the use of this cartridge and/or failure to
wear the respirator during all times of exposure can reduce respirator effectiveness and may
result in sickness or death.
2. Before occupational use of these cartridges, a written respiratory protection program must be
implemented meeting all the requirements of OSHA 29 CFR 1910.134 such as medical
evaluation, training and fit testing and applicable OSHA substance specific standards. In
Canada, CSA standard Z94.4 requirements must be met and/or requirements of the applicable
jurisdiction, as appropriate.
3. The airborne contaminants which can be dangerous to your health include those so small that
you cannot see them.
4. Leave the contaminated area immediately and contact your supervisor if you smell or taste
contaminants or if dizziness, irritation, or other distress occurs.
5. Store the cartridges and respirator away from contaminated areas when not in use.
6. Dispose of used product in accordance with applicable regulations.
Use Limitations
3
1. These cartridges do not supply oxygen. Do not use in atmospheres containing less than 19.5%
oxygen.
2. Do not use when concentrations of contaminants
- are immediately dangerous to life or health,
- are unknown,
- are greater than 10 times the permissible exposure limit (PEL) with half facepiece
respirators and full facepiece respirators when qualitatively fit tested.
- are greater than 50 times the PEL with full facepiece respirators when quantitatively fit
tested, or
- exceed specific OSHA standards or applicable government regulations, whichever is lower.
3. Do not alter, clean (e.g. vacuum, wash, use compressed air), abuse or misuse these cartridges
and/or respirator.
4. Do not use with beards or other facial hair or other conditions that prevent a good seal between
the face and the sealing surface of the respirator.
Time Use Limitations
Replace cartridge in accordance with an established change schedule or earlier if smell, taste or
irritation from contaminants is detected.
Special Instructions for 3M Mercury Vapor or Chlorine Gas Cartridge
6009
3M™ Mercury Vapor Cartridges (6009 and 60929) are equipped with passive 3M™ End of Service
Life Indicators (ESLI). The color change indicator must be readily visible when wearing the
respirator without manipulation. If you cannot readily see the ESLI, do not use. The mercury vapor
cartridges must be discarded when the ESLI changes to the discard color found on the mercury
vapor cartridge label; or within 30 days of opening packaging; or when ESLI becomes dirty or
damaged; or when odors of vapors or gases become noticeable, whichever occurs first. Mercury
vapor has no odor.
NIOSH approval: See NIOSH approval label insert.
FOR MORE INFORMATION
In United States, contact:
Website: www.3M.com/OccSafety
Technical Assistance: 1-800-243-4630
For other 3M products:
1-800-3M-HELPS or 1-651-737-6501
3M Occupational Health and
Environmental Safety Division
3M Center, Building 0235-02-W-70
4
St. Paul, MN 55144-1000
©3M 2011
98-0060-0065-1/4

Products related to this Datasheet

OV ACID GAS CARTRDG 1=1BAG(2PCS)
Available Quantity: 0
Unit Price: 0
ORGANIC VAPOR CARTRIDGE 1=1PAIR
Available Quantity: 0
Unit Price: 0
MULTIPLE GAS CARTRDG 1=1PAIR/BAG
Available Quantity: 175
Unit Price: 16.28
FORMALDEHYDE ORGNC VPR CRT 1=1PC
Available Quantity: 50
Unit Price: 18.32
AMMONIA METHYLAMINE CRTRD 1=1BAG
Available Quantity: 0
Unit Price: 0
ACID GAS CARTRIDGE 1=1PC
Available Quantity: 20
Unit Price: 16.62
70071622248 6009SCARTRIDG 1=1BAG
Available Quantity: 0
Unit Price: 0