Time Machine II Quick Start Guide Datasheet by SiTime

View All Related Products | Download PDF Datasheet
ETime" mm m mun .HBtFramework w‘wm MICROSOFI SOFTWARE SUPPLEMENIAL h...h.y.,.n..m._mu <9 0.an="" kmmumummm!="" mm="" hangman-mm»="" m="" ”ww...="" "mum...="" mm="" mm="" ”w="" hams...“="" mm.“="" mama="" _e="" installing="" device="" driver="" software="" ‘\="" x="" (idlluelovm="" usb="" input="" device="" “="" x="" devin="" «in:="" mm:="" inmlkd="" mummy,="" sunni"="" nun-m...="" ,="" mum“="" 5m...="" ne'rfmmklssemeu="" nu.="" mum.="" ducumnmulnn="" ,="" w="" ,="" u.="" m...="" ,="" wild-mm:="" w...="" rename)="" rm="" “a.“="" mm“="" m="" hwy-all:="" ummmm="" ,="" 5.1m.="" mam="" sewn="" m="" wm="" “was.“="" hmm="" :="" mu="" swam="" mm“.="" would="" you="" like="" lo="" install="" this="" device="" schware?="" nam:="" 51m="" why-1m="" “kw="" pubixhc:="" mm="" mp="" m="" ”mama-mush“:="" u="" vwmuumnmmmmlmwmwum="" um“="" ,="" .="" ,="">
Register your Time Machine II programmer at:
http://www.sitime.com/time-machine-registration
Time Machine II
MEMS Oscillator Programmer
QUICK START GUIDE
Kit Contents
• MEMSOscillatorProgrammer
• Socketcard(s)
• USBcable
• Tweezers
• Fieldprogrammabledevicesamplepacks
Step 1: Install Time Machine Software
•
Microsoft.NETFrameworkmustbeinstalledontargetcomputer.
•
Gotohttp://www.sitime.com/tm-sw,downloadSiTimeinstaller
packageontotargetcomputerthatcontainsTimeMachineII
softwareinstaller,license,userguidesandotherdocumentation.
•
RuntheSiTimeinstallerexecutable,andthefollowingGUIwill
appear on screen:
For Microsoft® Windows XP operating system only
•
.NETFramework4.0ServicePack1mustbeinstalled.During
the driver installation process, you may be prompted to
install.NETFramework4.0.
•
Downloadandinstall .NETFramework4.0 fromtheMicro-
softDownloadCenterathttp://bit.ly/1OD2tMH.
• After.NETFrameworkisinstalled,presstheInstallbutton
nexttoTime Machine Softwaretostartinstallation.
• ReadandaccepttheLicenseAgreementandfollowthe
onscreeninstructionstocompletetheinstallation.
• ClickontheSiTime Time Machine icon to start the Time
Machinesoftware.
• TimeMachinedriverinstallationisrequiredduringfirst
use.SelectAlways trust software from “sitime corp”and
press the Installbutton.
• Connected and READY will be displayed in the bottom
leftcorneroftheTimeMachine windowto confirmthat
the programmer status is ready to run (See screen on
nextpage).
Step 3: Launch
Time Machine Software
• ConnecttheSiTimeprogrammertoyourPCwiththeUSB
cable.
• Check that the power light on the SiTime programmer
is illuminated. The red light is located under the Time
Machine IIlabelontheprogrammer.Ifthepowerlightdoes
notappear,makesuretheUSBportonthePCisactive.
• TheWindows Found New Hardware notification willauto-
maticallyappearonscreen.WaituntiltheUSBdevicedriver
installationiscompletebeforecontinuing.
Step 2: Connect the
MEMS Oscillator Programmer
For Microsoft® Windows Vista 7/8/10 operating systems
RefertotheGUIscreenonpage1forthefollowinginstructions.
•
If .NET Framework 3.5 SP1 is installed on your computer, a
greencheckmarkwillappearnexttothe.NET Framework 3.5
Service Pack 1 line under Software Installation and the Install
buttonwillbegrayedout.
•
If .NET Framework 3.5 SP1 is NOT installed on your computer,
clicktheInstallbuttonwhichwillbegintoextracttherequired.NET
Framework setup files included with SiTime Installer download
package. Read and accept .Net Framework License Agreement
andfollowonscreeninstructionstocompletetheinstallation.
Mmm—M new me. A Yuum: m mummu. («Dun—mm
• PresstheProgrambuttontoprogramthedevice.
Step 4: Program MEMS Oscillators
• Select and insert the socket card for the oscillator
packagesizeyouneed.
• Each socket card has two sockets for different pack-
age sizes. Use the tweezers to insert a field program-
mabledeviceintothepropersocketonthesocketcard.
Align pin 1 (which is indicated with a small circle on
top of package) with the small white triangle on the
socketcard.
• EntertheSiTimepartnumberintothepart numberfield
in the programming software window. Or use the Part
Number GeneratortobuildtheSiTimepartnumber.
• WhenthegreenPASSEDindicatorisdisplayedatthebot-
tomoftheTimeMachineIIwindow,youhavesuccessfully
programmedtheSiTimeMEMSoscillator.Congratulations!
Notice to Users
1. The Time Machine II Programmer and associated hardware (henceforth Platform)
are intended for use only with SiTime’s MEMS oscillators. This Platform will not
program any other manufacturer’s programmable oscillators and no attempt to do
so should be made.
2. The Platform is intended for use for engineering development and evaluation of
SiTime’s MEMS Oscillators. SiTime does not guarantee or warranty the devices that
are programmed on this Platform for qualification or production purposes.
3. The Platform should be used in a static free environment with good engineering
practices.
4. This Platform does not fall under the scope of the European Union directives
regarding electromagnetic compatibly, FCC, CE or UL and therefore may not meet
the technical requirements of these directives.
5. THE PLATFORM AND ITS ACCOMPANYING SOFTWARE AND DOCUMENTATION ARE
PROVIDED ON AN “AS-IS” BASIS, “WITH ALL FAULTS”, AND WITH NO WARRANTY
WHATSOEVER. SITIME AND ITS LICENSORS EXPRESSLY DISCLAIMS ALL WARRANTIES,
WHETHER EXPRESS, IMPLIED OR STATUTORY, INCLUDING WITHOUT LIMITATION ANY
WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE, TITLE,
AND NON-INFRINGEMENT. SITIME DOES NOT WARRANT THAT USE OF THE PLATFORM
(OR ITS ACCOMPANYING SOFTWARE) WILL BE UNINTERRUPTED OR ERROR-FREE OR
THAT DEFECTS WILL BE CORRECTED OR THAT THE PLATFORM (OR ITS ACCOMPANYING
SOFTWARE) ARE FREE OF VIRUSES OR OTHER HARMFUL COMPONENTS.
6. The user assumes all responsibility and liability for [the] proper and safe handling of
the Platform and the associated programmed MEMS Oscillators.
7. The user indemnifies SiTime from all claims arising from the handling or use of this
Platform and the associated field programmable devices.
8. Please contact a SiTime representative if you have any issues or problems with
using this Platform.
© 2015 SiTime Corporation. All rights reserved.

Products related to this Datasheet

MEMS OSCILLATOR PROGRAMMER
Available Quantity: 2
Unit Price: 304.8