TechZone
Lighting Solutions
High Power LEDs : 1 A - 2.8 A test

This section contains discrete LEDs with current ratings from 1 A to 2.8 A. The LEDs are subdivided by wavelength into color groups. To use this section, select a color from one of the options below and click on the Compare Product Specifications link. In addition, specific products are listed below for each color category.

A second option is the Parametric Search which can be used to view all LEDs in this section.


LED Color Options

  • Warm White
  • Neutral White
  • Cool White
  • Red, Green, Blue (RGB)
  • Blue
  • Green
  • Yellow
  • Red
Warm White

These LEDs have a correlated color temperature between 2500 K and 3699 K which correspond to the visible colors generally classified as warm white. These color temperatures are outlined on the C.I.E. Diagram.


Cree, Inc. - MC-E

Cree, Inc. - MC-EThe XLamp MC-E LED is a lighting-class multi-chip LED that provides 4 times the flux as XLamp XR-E in the same footprint, without compromising thermal performance. XLamp MC-E reduces LED system cost by reducing system complexity and the number of components required.

Pricing & Availability
Neutral White

These LEDs have a correlated color temperature between 3700 K and 4999 K which correspond to the visible colors generally classified as neutal white. These color temperatures are outlined on the C.I.E. Diagram.


Cree, Inc. - MC-E

Cree, Inc. - MC-EThe XLamp MC-E LED is a lighting-class multi-chip LED that provides 4 times the flux as XLamp XR-E in the same footprint, without compromising thermal performance. XLamp MC-E reduces LED system cost by reducing system complexity and the number of components required.

Pricing & Availability
Cool White

These LEDs have a correlated color temperature between 5000 K and 8000 K which correspond to the visible colors generally classified as cool white. These color temperatures are outlined on the C.I.E. Diagram.


Cree, Inc. - XR-E

Cree, Inc. - XR-EThe XLamp XR-E LED is leading the LED lighting revolution with its unprecedented lighting-class brightness, efficacy, lifetime and quality of light. These lighting-class features enable the XLamp XR-E LED to replace many traditional light sources and save money with energy-efficient light and long lifetimes.

Pricing & Availability

Cree, Inc. - MC-E

Cree, Inc. - MC-EThe XLamp MC-E LED is a lighting-class multi-chip LED that provides 4 times the flux as XLamp XR-E in the same footprint, without compromising thermal performance. XLamp MC-E reduces LED system cost by reducing system complexity and the number of components required.

Pricing & Availability
Red, Green, Blue (RGB)

These LEDs combine red, green, and blue dies into one package. The intensity of each color can be independently controlled to generate a wide range of colors in the visible spectrum.


TT Electronics/Optek Technology - Optimal X

TT Electronics/Optek Technology - Optimal XThe OVTL09LG3x Series surface mount provides a 10-Watt energy-efficient 3-dimensional packaged LED source that offers high luminance, low thermal resistance @ 2.5°C/W and a long operating lifespan.

Pricing & Availability
Blue

These LEDs have wavelengths between 428 nm and 491 nm which correspond to visible colors in the blue spectrum as shown on the C.I.E. Diagram.


Cree, Inc. - XR-E

Cree, Inc. - XR-EThe XLamp XR-E LED is leading the LED lighting revolution with its unprecedented lighting-class brightness, efficacy, lifetime and quality of light. These lighting-class features enable the XLamp XR-E LED to replace many traditional light sources and save money with energy-efficient light and long lifetimes.

Pricing & Availability
Green

These LEDs have wavelengths between 492 nm and 575 nm which correspond to visible colors in the green spectrum as shown on the C.I.E. Diagram.


OSRAM - Diamond Dragon

OSRAM - Diamond DragonDiamond Dragon LEDs are designed for use in office and residential lighting as well as automotive, industrial and signage applications. Positioned between the 3-watt Platinum DRAGON and the 10-watt OSTAR, they come in the complete range of colors. They have exceptional output, excellent thermal management, and durability.

Pricing & Availability
Yellow

These LEDs have wavelengths between 576 nm and 596 nm which correspond to visible colors in the yellow spectrum as shown on the C.I.E. Diagram.


OSRAM - Diamond Dragon

OSRAM - Diamond Dragon Diamond Dragon LEDs are designed for use in office and residential lighting as well as automotive, industrial and signage applications. Positioned between the 3-watt Platinum DRAGON and the 10-watt OSTAR, they come in the complete range of colors. They have exceptional output, excellent thermal management, and durability.

Pricing & Availability
Red

These LEDs have wavelengths between 620 nm and 780 nm which correspond to visible colors in the red spectrum as shown on the C.I.E. Diagram.


OSRAM - Diamond Dragon

OSRAM - Diamond DragonDiamond Dragon LEDs are designed for use in office and residential lighting as well as automotive, industrial and signage applications. Positioned between the 3-watt Platinum DRAGON and the 10-watt OSTAR, they come in the complete range of colors. They have exceptional output, excellent thermal management, and durability.

Pricing & Availability

TT Electronics/Optek Technology - Optimal X

TT Electronics/Optek Technology - Optimal XThe OVTL09LG3x Series surface mount provides a 10-Watt energy-efficient 3-dimensional packaged LED source that offers high luminance, low thermal resistance @ 2.5°C/W and a long operating lifespan.

Pricing & Availability


Lighting Suppliers - 1 A to 2.8 A High Power LEDs